The following table lists the predefined types and their description:
| Type | Description | Supported for |
|---|---|---|
| byte | 8-bit unsigned integer (unsigned char) | all |
| bool | Boolean value (unsigned char) (TRUE = any non-zero value / FALSE = 0) | all |
| word | 16-bit unsigned integer (unsigned int) | all |
| dword | 32-bit unsigned integer (unsigned long) | all |
| dlong | array of two 32-bit unsigned integers (unsigned long) | all |
| TPE_ErrCode | Error code (uint8_t) | all except MPC55xx |