Timing setup problems

The errors are reported in red in the Timing dialog or in the timing property line in the Component Inspector. The error summary is available in the Error window. Follow the error message text to find the source of the problem. If no error is reported, it means that Processor Expert can achieve the desired timing for all components in the project.

Common problems that make impossible to set a timing value: