TimeDate component

It is recommended to set a resolution to multiples of 10 ms (resolution of the time provided by the GetTime/ SetTime methods). It should be 10ms or more. Smaller values are unnecessarily overloading the system.