These devices are simple counters that do not contain multiple individually configurable channels and usually do not allow to control any pins. These devices cannot be shared (that is used by multiple components).
The following devices are members of this group:
These devices are usually listed in Processor Expert under their original names without any extensions. These devices can be used by the following high-level components: TimerInt , RTIshared , TimerOut and FreeCntr8/16/32. The MTIM peripheral can additionally be used in event counter components (EventCntr8/16/32). All peripherals from this group are also supported by the Peripheral Initialization Components (Component categories).