PulseAccumulator component

This component is generally used to count pulses (events) generated on external inputs. Thus, the primary and secondary input can only be a physical pins of the device. The primary input is required to be an internal clock, the Init_TMR component should be used.