Processor properties overview

Processor properties can be set in processor Component Inspector view. The complete list of processor properties and their description is available in the help page for the processor. To open the processor help page, select Help > Help on Component from the menu bar in the Component Inspector view.

Following properties define the basic settings of the processor: