Processor Expert files and directories

All components in the project with their state and settings and all configurations are stored in one file ProcessorExpert.pe in the root of project directory. If the whole content of the project including subdirectories is copied or moved to another directory, it is still possible to open and use it in the new location.