It is possible to use Processor Expert to generate only the initialization code (function) for a peripheral using the Peripheral initialization components. You can choose a suitable Peripheral initialization component for the given peripheral using the Peripherals tab of the Components Library. See Components Library view topic for details. Initial values that will be set to the peripheral control registers can be viewed in the Peripheral Initialization window. See Configuration Registers view topic for details.