OnReset event

You can write the code that will be invoked from the PE_low_level_init() function after Processor Expert internal initialization, but before the initialization of individual components. Thus, you should expect that peripherals are not completely initialized yet. This event can be enabled/disabled in the processor component inspector's events page.