Multi-channel timer peripherals

These timer peripherals provide multiple channels and allow several modes of operation.

The following devices are members of this group:

Processor Expert shows each of these timer peripherals as multiple devices that can be used by the components. The name of such device (shown in the peripheral selection list) consists of the peripheral and a suffix specifying the part of the peripheral or it's specific function. These named devices represent the whole peripheral or parts of the peripheral set to work in a specific mode. Using only a part of the timer allows to share the timer by multiple components.

The following devices are usually defined for the complex timer peripherals:

(the examples are for the MC68HC908AZ60 processor)