Processor Expert always checks the usage of the internal and external memories accessible through processor address and data bus. Position and size of internal memory is defined by the processor type and can be configured in the processor Properties (if supported). External memories must be defined in processor Properties.
Any component can allocate a specific type of memory. Processor Expert provides checking of memory and protects you from making a wrong choice. For example, if a component requires external Flash, it is not possible to enter an address in internal RAM.
The bits can also allocate memory. Therefore, you can be sure that only one component uses an allocated bit of a register in external address space.