In some cases, a non-standard use of the peripheral is required and it is more efficient to write a custom peripheral driver from scratch than to use the component. In addition, there are special features present only on a particular chip derivative (not supported by the component) that could make the user routines more effective; however, the portability of such code is reduced.