Logical Device Drivers were developed to offer users the Hardware Abstraction Layer (HAL) for bare-metal applications as well as RTOS applications. The components provide tested, optimized C code tuned to the application needs. The code may be tuned to the specific RTOS when the RTOS component is in the project.