Interrupt handling

Some Peripheral Initialization components allow the initialization of an interrupt service routine. Interrupt(s) can be enabled in the initialization code using appropriate properties that can be usually found within the group Interrupts.

After enabling, the specification of an Interrupt Service Routine (ISR) name using the ISR name property is required. This name is generated to Interrupt Vector table during the code generation process. Please note that if the ISR name is filled, it is generated into the Interrupt Vector Table even if the interrupt property is disabled.

Figure 1. Example of the interrupt configuration

Enabling/disabling peripheral interrupts during runtime has to be done by user's code, for example by utilizing PESL or direct register access macros, because the Peripheral Initialization Components do not offer any methods for interrupt handling.

The ISR with the specified name has to be declared according to the compiler conventions and fully implemented by the user.

Note: For 56800/E version users: ISRs generated by Processor Expert contain the fast interrupt handling instructions if the interrupt priority is specified as fast interrupt.