Sometimes, there is unwanted any change in the code generated by Processor Expert. It's for example in case of manual modification done by the user and the user doesn't want to loose the code by accidental re-generation of PE project. For such cases there is an option in Processor Expert Project Options that completely disables the code generation. See Processor Expert options for details.