Events

Some components allow handling the hardware or software events related to the component. You can specify the name on function invoked in the case of event occurrence. They are usually invoked from the internal interrupt service routines generated by Processor Expert. If the enabled event handling routine is not already present in the event module then the header and implementation files are updated and an empty function (without any code) is inserted. You can write event handling code into this procedure and this code will not be changed during the next code generation.

All Methods and Events of each component inserted into the project are visible as a subtree of components in the Components view.