This topic describes how the size and speed of the code could be optimized by choosing right component for the specific task. It also describes how to setup components to produce optimized code. The optimizations that are described are only for the High or Low level components, not for the Peripheral Initialization components.
For more details, refer to the following topics: