Creating user component templates

If you frequently use a component with the same specific settings, you may need to save the component with its settings as a template. This template is displayed in the Components Library view under given name, behaves as a normal component and could be added to any project. The template has the same properties as the original component. The value of the properties are preset in the template and could be marked as read only.

This topic describes how to create a component template and save it.