You can let Processor Expert call the Init method automatically by selecting "yes" for the Call Init method in the Initialization group of the Component's properties.
When this option is set, Processor Expert places the call of the Init method into the PE_low_level_init function of the CPU.c module.