Apply board configuration

You can import board configuration from a file. The imported configurations are added into the selected project.

To import board configuration:

  1. In the IDE, select File > Import. The Import wizard appears.

    Expand Processor Expert tree. Select Apply Board Configuration option as shown below.

    Figure 1. Import wizard

  2. Click Next. The Apply Board Configuration page appears.
    Figure 2. Apply board configuration page

    Before importing, you can rename some of the components (as shown in figure above), so it will show the mapping of components with different names, but same device allocation.

    To import component settings from the file to selected project, click the Browse button. Select the input file with the .peb extension. The default option Replace settings is selected if imported component settings are having same peripheral device allocation (or ID) and type.

    For more information on different types of modes, see Component settings to project topic.

  3. Click Finish. The settings from the .peb file is imported to the selected project.

You are ready to import board configuration.