Adding a processor to a project
- In the Components Library view, select the Processors tab and find the desired processor component.
- Double-click the desired processor icon to add it to the project. When the processor component is added, it appears in the upper part of the Components view. If selected as the target processor, the processor will be displayed in the Processor view.