Timing precision configuration

It is possible to specify desired precision of the timer settings by using one of the following settings (which one is used depends on the type of the timing):

In case of interval settings type, the % of low limit (percentage of the low limit value) can be used as the unit for this value.