Syntax for the timing setup in the Component Inspector

The properties that contain timing settings can be configured using the timing dialog (For details, see Dialog for timing settings topic) or directly entering the timing value. If the timing values are specified directly, it is necessary to enter not only a value (integer or real number) but also the unit of that value. The following units are supported:

For example, if you want to specify 100 milliseconds, enter 100ms.

For more details on timing configuration, see Timing settings topic.