This menu is available on right-clicking at the ProcessorExpert.pe file. It contains the standard CodeWarrior commands with the Processor Expert specific command:
Generate Processor Expert Code - Invokes code generation for the current project. The generated files are automatically inserted into the active (default) target in the CodeWarrior's project. Generated files corresponding to the Embedded Components can be accessed from the Generated_Code folder. For more details, see Code Generation topic.
For Processor Expert related settings and options, see Processor Expert Options.