Possible settings table

This table is displayed on the right side of the timing dialog when you click the Possible settings button on the top. The table displays values supported by the Processor for the selected peripheral.

If there are only individual values available to set, the table contains a list of values, each row represents one value. If there are intervals with a constant step available, each row contains one of the intervals with three values: From , Till - minimum and maximum value, Step - a step between values within the interval.

The way the values are displayed may be dependent on:

By clicking on the table header, there is possible to order the rows as per selected column. By clicking the same column again, you can arrange the rows in ascending or descending order.

Double-clicking on a value will place the value into the currently edited row within the Timing values table.

The values listed in the possible settings table depend on the following timing settings:

and it also depends on

The table contains a speed mode tabs (speed modes and related settings are supported only in the Expert view mode) that allow to filter the displayed intervals for a specific speed mode or show intersection of all. Note that the intersection contains only values that can be set in all speed modes with absolute precision (without any error), so some values that are still valid, but due to non-zero Error allowed, values are not shown.