The menu content is specific for selected item. This is the popup menu for Processors.
-
Inspector
- opens
Component Inspector
view for the component. For more details, see Component Inspector view topic.
-
Inspector - Pinned
- opens
Component Inspector
view for the component in "pinned" mode. This command allows to have several inspector views for different components opened at once. For more details, see Component Inspector view topic.
-
Code Generation
- allows to disable/enable the generated module for the component and CPU component.
-
Configuration Registers
- displays the
Configuration Registers
view for the peripheral initialized by the selected component. For more details, see Configuration Registers view topic.
- Target Processor Package - displays the
Processor
view for the processor derivative used in a given project.
- Processor Memory Map - displays the
Memory Map
view for the processor address space and internal and external memory mapping.
- Rename Component - changes the name of the component.
- Select
Distinct/
Shared mode
- switches between shared and distinct mode of the component. This setting is available for LDD components only. For more details, see Logical Device Drivers topic.
- Open File
- opens the generated code from the selected component for the source code editor. Note that the code is available only after successful code generation.
-
Component Enabled
- enables/disables component in the project.
- Copy/Paste
- components can be copied and pasted inside the same project, between two projects in the same workspace, and between two projects having each project in separate workspace.
-
Remove component from project
- deletes the component from the project.
-
Help on component
- shows a help page for the component.
-
Save Component Settings As Template
- creates a template of the selected component. For more details, see Creating user component templates topic.
- Hot key
Delete
is used for deleting components from the project.
-
View Code
- Opens code editor at the code of the selected method or event.
- Toggle Enable/Disable
- Enables/Disables the Method or Event.
Figure 1.
Components view