Modes

The Components Library has the following four tabs allowing you to select components in different modes:

Component names are colored black and the component template names are colored blue. The components that are not supported for the currently selected target processor are gray. By double-clicking on the component, it is possible to insert the component into the current project. The description of the component is shown in a hint.