Minimal timer ticks

Note: This item is available only for setting of period in components where it is meaningful, for example PWM, PPG.

It represents requirement for minimal number of timer ticks for specified period (usually it affects minimal value set into reload or modulo register). This is useful for configurations where it is expected to change period or duty in runtime, and in this case the parameter affects supported scale for such changes. There will be guaranteed that there will be at least the given number of distinct values available for adjusting the duty of output signal. This will also be guaranteed for any available period of the signal.