Memory Map view

To open this view, click Window > Show View > Other... and select Processor Expert > Memory Map.

Figure below shows the processor address space and internal and external memory mapping. Detailed information for an individual memory area is provided as a hint when you move the cursor over it.

Table 1. Legend
Legend Description
white: non-usable space
dark blue: I/O space
blue: RAM
light blue: ROM, OTP or Firmware
cyan: FLASH memory or EEPROM. This area can also contain a flash configuration registers area.
black: external memory

The address in the diagram is increasing upwards. To improve the readability of the information, the size of the individual memory blocks drawn in the window are different from the ratio of their real size (small blocks are larger and large blocks are smaller).

The black line-crossed area shows the memory allocated by a component or compiler. The address axis within one memory block goes from the left side to the right (it means that the left side means start of the block, the right side means the end).

Figure 1. Sample of used part of the memory area