Items visibility

Processor Expert supports selectable visibility of the component items. Each item is assigned a predefined level of visibility. Higher visibility level means that items with this level are more special and rarely used than the others with the lower visibility level. Component Inspector displays only items on and below the selected level. It could help especially beginners to set only basic properties at first and do optimization and improvements using advanced and expert properties or events later. There are three visibility levels:

The visibility can be switched in the Component Inspector using Basic, Advanced, and Expert buttons or within its view menu.

Note: If an error occurs in a property with a higher visibility level than the level currently selected, then also this error is displayed.