Filtering

Filter can be activated using the filtering icon. If it is active, only the components that could be used with the currently selected target processors are shown.

If the filter is inactive, Processor Expert also shows components that are not available for the current processor.