Control buttons

The following table lists and describes the control buttons:

Table 1. Control buttons
Buttons Description
Zoom in - Increases the detail level of the view. The whole picture might not fit the viewing area.
Zoom out - Decreases the detail level of the view. Processor Expert tries to fit the whole picture to the viewing area.
Rotate - Rotates the package clockwise.
Resources (available for BGA type packages only) - Selects Resources view mode that shows a top side of the package without pins but including list of peripherals and showing their allocation by components.
Pins Bottom (available for BGA type packages only) - Selects Pins view mode that shows a bottom side of the package with pins. The peripherals are not shown in this mode because the surface is covered with pins.
Pins Top - Selects Pins view mode that shows a top side of the package with pins.