Components view

To open this view, click Window > Show View > Other... and select Processor Expert > Components.

Components view shows the tree with the following items:

Note: PESL and PDD folders are available only for Peripheral Initialization components and only if PDD library or PESL library is supported for the selected processor. Either PESL or PDD folder is displayed and not both.
Figure 1. List of PDD macros

All component's items have status icons that signify the enabled or disabled state. If this state cannot be changed directly, the background of the icon is gray. For more details, see Embedded components topic.

This table explains the various states of a component.

Table 1. Description of component states
Component Status Icon Description
Signifies that component is enabled. It can be configured and code can be generated from this component.
Signifies that component is disabled. It can be configured, but the configuration validation/ generation is disabled. No code is generated from this component.
Signifies error in the component. For example, Components folder contains component with error.
Signifies that component is frozen and will not be re-generated. When the user generates the code again, files of this component are not modified and the generated code is frozen.

Shared components are automatically placed into a dedicated subfolder Referenced_Components. You can move the component from this folder to anywhere.

Figure 2. Referenced components

When you have more than one Processor Expert project in your workspace and you are working with those projects, the last project shown in Components view is recorded in the workspace history. When you restart the Eclipse IDE, the last session project is opened automatically.