There are exciting possibilities in starting a new project if the user is starting from ground zero even if the user is using a new and unfamiliar processor.
- You can work on microcontroller immediately without studying about the microcontroller
- Documentation
- You can implement simple applications even without deep knowledge of programming
- PE presents all necessary information to the user using built-in descriptions and hints
- PE has built-in tutorials and example projects.