Integrated development environment increases productivity:
- This tool lets you produce system prototypes faster because the basic setup of the controller is easier. This could mean that you can implement more ideas into a prototype application having a positive effect on the specification, analysis, and design phase. PE justifies its existence even when used for this purpose alone.
- This system frees you up from the hardware considerations and allows you to concentrate on software issues and resolve them.
- It is good for processors with embedded peripherals. It significantly reduces project development time.
The primary reasons why you should use Processor Expert are:
- Processor Expert has built-in knowledge (internal definition) of the entire microcontroller with all its integrated peripherals.
- Processor Expert encapsulates functional capabilities of microcontroller elements into concepts of configurable components.
- Processor Expert provides an intuitive graphical user interface, displays the microcontroller structure, and allows you to take the advantage of predefined and already verified components supporting all typically used functions of the microcontroller.
- Applications are designed by defining the desired behavior using the component settings, drag and drop selections, utilizing the generated methods and events subroutines, and combining the generated code with user code.
- Processor Expert verifies the design based on actual microcontroller resource and timing contentions.
- Processor Expert allows the efficient use of the microcontroller and its peripherals and building of portable solutions on a highly productive development platform.