Processor Expert static code repository

Processor Expert installation directory contains static code repository with static driver modules for all supported processors. Projects in linked mode shares the repository and repository content is used when new standalone project is created. See Standalone and linked project topic for more information about standalone and linked mode.

Processor Expert static code repository is divided into sub-folders with one processor family support in each of them. It is placed at: {CodeWarrior}\Processor Expert\lib\{Processor family} and has the following sub-directories: