Complete set of static drivers is stored directly in the project directory. During project creation, static drivers are copied from shared static code repository to the project repository.
After project is created, it is independent from development environment and from other projects therefore changes made in static drivers in one project don't affect rest of the projects. It is possible to synchronize project's local repository with the common one. Processor Expert detects changes in the common repository, informs user about them and offers project local repository update. Also, if static driver is missing in the project directory but is required by Embedded Component used in the project then Processor Expert offers adding of the missing files.