Timing settings

Timing settings are vital part of functionality of some peripherals. For example, in case of timer peripheral, it would be period of counter overflow, conversion time of analog-to-digital converter or baud rate of communication interface. Configuration of these features in the high-level and LDD components is done in the Timing Settings dialog. This user-friendly interface allows configuration of peripheral timing settings. Generally, user can specify required timing value directly or pick up the suitable value from list of values computed according to current settings. For detailed documentation, see Dialog for Timing Settings topic and Timing Settings topic.

In following topics, the relation between timing settings and clock configurations are discussed.