Use the ARM Ltd Windows GCC C Compiler panel to specify the compiler options that are specific to the ARM (GCC).
The following figure shows the ARM Ltd Windows GCC C Compiler panel.
The table below lists and describes the various options available on the ARM Ltd Windows GCC C Compiler panel.
| Option | Description |
|---|---|
| Command | Shows the location of the compiler executable file. Default: arm-none-eabi-gcc |
| All options | Shows the actual command line the compiler is called with. |
| Expert settings | Shows the expert settings command line parameters. Default: " ${ARMSourceryDir}/${COMMAND}" ${INPUTS} ${FLAGS} ${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT}" |
| Command line pattern |