What does Critical Code data display?

The critical code data displays the summarized data of a function in a tabular form, such as name of the function that is executed, start address of the function, number of lines executed in the function, and number of clock cycles taken by the function.

The critical code data is displayed in the Critical Code viewer that is divided into two parts. The upper part displays the summary of the functions, and the lower part displays the statistical details of all the instructions executed in a function.