What are start and stop triggers/tracepoints?

A start trigger/tracepoint starts the trace collection from the address where it is set. A stop trigger/tracepoint stops the trace collection at the address where it is set. You can set trigger A as start trigger and trigger B as stop trigger and vice-versa. A trigger is set on the HCS08 or ColdFire V1 target, and a tracepoint is set on the Kinetis target.