In the CodeWarrior for Microcontrollers v10.1, the trimming functionality is available in the
PEMicro
menu of the IDE menu bar. Whereas, in the CodeWarrior for Microcontrollers v10.2 or higher, you can access this functionality from
Debug/Run Configurations
dialog box. To trim a microcontroller follow the steps listed below:
- Select Debug Configurations from the IDE menu bar.
The
Debug Configurations
dialog box appears.
Figure 1. Debug Configurations Dialog Box 
- Click Edit from the Connection group.
The
Properties for <project_name>
dialog box appears.
Figure 2. Properties for <project_name> Dialog Box 
- Click Advanced Programming Options from the Connection tab.
The
Advanced Options
dialog box appears.
Figure 3. Advanced Options Dialog Box 
- Check the Use custom trim reference frequency checkbox and specify the desired trim frequency for your microcontroller.
Note: The trimming feature is not supported for all microcontroller devices.