In order to compile the project, follow steps below:
A context menu appears.
If Build Automatically is checked, then when Clean Project executes, it creates a Binaries folder that contains the *.abs file that are used for debugging. If Build Automatically is unchecked, then Clean Project removes any previously-built binaries, including the *.abs file.
The project compiles.