The example projects are available at the following location:
<install_dir>\MCU\CodeWarrior_Examples
, where
<install_dir> refers to the CodeWarrior installation directory.
Additional Example Projects are available on the Web. They can be found in the
Self-Paced Training
section on the
Training & Support
tab of the CW MCU Web page.
http://www.freescale.com/webapp/sps/site prod_summary.jsp?code=CW-MCU10&tab=Design_Support_Tab)
-
Processor Expert Example Project for TWR-K60N512: Includes a CW MCU v10.1 project using Processor Expert to create a bare board (no RTOS) application to use GPIO and Timers to blink LEDs on the TWR-K60N512 board. It also includes the step by step instructions to recreate the project.
-
Example Projects for TWR-K40X256-KIT and TWR-K60N512-KIT: Includes CW MCU v10.1 bare board (no RTOS) projects for TWR-K40X256-KIT and TWR-K60N512KIT. The projects for each kit include: adc_demo, can_loopback_node, crc_demo, dac12bit_demo, flexbus, flexmem, gpio, hello_world, hscmp, i2c, lptmr, mcg_demo, pdb_adc_demo, pmc, rtc, sci2can, slcd, tsi, USB_DCD, USB_device, USB_dual_role, USB_HOST, USB_MAX3353.