The projects that reference s Explorer (RSE) Systems contain an internal cache of the referenced RSE Systems. When such projects are imported in the workspace, the RSE settings in the cache may differ from the actual RSE settings in the workspace. Or the RSE settings may be missing entirely from the project.
In such situations, the Changed dialog box appears.
The RSE settings are stored in the .metadata workspace folder as a part of the project settings and in the rseHostSettingsCache.xml file (refer to the image listed below), as the cached version, in the project.
As with any cache, the cache might be out of sync or needs to be flushed, which causes a mismatch between the RSE settings in the cache and the actual RSE setting in the project.
To resolve the issue, you need to configure the merge settings.
To configure IDE's response when an RSE system mismatch is detected, perform the following steps:
Alternatively, select Window > Preferences from the CodeWarrior menu bar. In the Preferences dialog box, select s > Merge .
The Merge page appears in the Preferences dialog box.
The merge settings are configured.