FAQs - Project Management
In this topic:
How can I find out where the source files related to a CodeWarrior project are saved?
How can I add another source or header file to my project?
What is a workspace?
What is a project?
How can I view the contents of various types of source code files that appear in my project folder?
Is there a way to compare the Property Settings of two different projects?
How do I resize the various views in a Perspective?
How can I add a project from some other workspace to my current workspace?
How do I ensure that the CodeWarrior IDE saves all modifications that I make to the project properties?
While working with the CodeWarrior IDE, the Remote System Changed dialog box appears. Why does it appear and how can I resolve the issue?
Which set of files I need to backup or store in a version control system to completely recover project settings and related debug settings?
I need to share a project without using a version control system. Is there any way to do this?
While importing a project, is there any way to find out which file mapping are missing?