Updating and Installing Software
In this topic, installation related FAQs are listed.
I have installed CodeWarrior for Microcontrollers on Linux Ubuntu 8.04, 64-bit. However, Multilink drivers are not working. What do I do?
I want to install updates for the CodeWarrior software. However, when I check for updates, no updates are found. What do I do?
I am facing issues in accessing the updater sites. How do I resolve this?
My attempt to install the CodeWarrior tool fails with the error "Another version of this product is already installed". What do I do?
How do I uninstall the third party plugins?
After updating the CodeWarrior, I receive the following error while restarting the application, "'Initialize RSE' has encountered a problem". What should I do?
How do I know what updates/patches are already installed?
I have installed the CodeWarrior patches on Windows 7. The patches have installed correctly, however the CodeWarrior software generates error while building the libraries. Is there any way to resolve this?
How can I check if the compiler updater is successfully installed?