Yes, working sets help reduce the number of resources displayed. A
working set is a group of elements you want to display.
To create or define a new working set, perform the following steps.
- Click
in the CodeWarrior Projects view or Project Explorer view toolbar. The pull-down menu appears.
- Select the Select Working Set command.
The
Select Working Set
dialog box appears.
- Click the New button.
The
New Working Set
wizard appears.
- From the Working set type options, select the appropriate working set. For example, select C/C++.
- Click Next.
The
<selected> Working Set
page appears. For example,
C/C++ Working Set.
- In the Working set name field, enter an appropriate name for the working set. For example, Demo_Set.
- In the Working set content tree, check the items you want in your view. For example, check Project_1 and Project_3 (refer to the image listed below).
Figure 1. New Working Set Wizard - C/C++ Working Set Page 
- Click Finish to close the New Working Set wizard.
- The Select Working Set dialog box reappears with the newly created working set.
Figure 2. Select Working Set Dialog Box 
- Check the checkbox corresponding to the desired working set and click OK.
The
CodeWarrior Projects
view or
Project Explorer
view will now display the selected resources only.
Note: To deselect an active working set, select the Deselect Working Set command from the view pull-down menu.
Note: To edit an active working set, select the Edit Active Working Set command from the view pull-down menu.