I have installed the CodeWarrior patches on Windows 7. The patches have installed correctly, however the CodeWarrior software generates error while building the libraries. Is there any way to resolve this?

If you install patches under non-admin privileges, all looks like it goes well. It shows that the patches are installed. However, when you build the libraries, you still get the error. Also, there is no way to uninstall the patches so you can re-install them with the admin privileges.

There are two ways to work this around: