How can I improve the performance of the CodeWarrior IDE I am working with?

Yes, you can improve the performance of your CodeWarrior IDE by disabling the features that slow down the software.

  1. Disable Indexer Options
    1. From the CodeWarrior IDE menu bar, select Window > Preferences.

      The Preferences dialog box appears.

    2. Type index as the filter text to narrow down the list of preferences.
    3. Select C/C++ > Indexer.

      The Indexer page appears in the right panel of the Preferences dialog box.

    4. Clear the Enable indexer checkbox.
  2. Disable Scalability Mode Settings
    1. In the Preferences dialog box, type scalability as the filter text.
    2. Select C/C++ > Editor > Scalability.

      The Scalability page appears in the right panel of the Preferences dialog box.

    3. Clear the Enable all scalability mode options checkbox.
  3. Disable Content Assist Auto Activation
    1. In the Preferences dialog box, type content as the filter text.
    2. Select C/C++ > Editor > Content Assist.

      The Content Assist page appears in the right panel of the Preferences dialog box.

    3. Clear all checkboxes in the Auto-Activation section.
  4. Click OK.

The performance of the CodeWarrior IDE improves.